Other Parts Discussed in Thread: UCC33420, UCC33020, UCC33010
Tool/software:
e2e,
Would you please recommend a solution to replace ADUM3260? Is something like UCC33410 + ISO1640B be the best replacement?
Thank you,
Adam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Adam,
Depending on your input and output voltage specs you can use:
UCC33420: 5V/5V with an option for 5.5V, 1.5W nominal output power @Ta=25C.
UCC33410: 5V/3.3V with an option for 3.7V, 1W nominal output power @Ta=25C
UCC33020: 3.3V/5V with an option for 5.5V, 1W nominal output power @Ta=25C
UCC33010: 3.3V/3.3V with an option for 3.7V, 1W nominal output power @Ta=25C
For questions regarding ISO1640B, please summit another e2e with that part number. An engineer expert will reach out to you.
Thank you