This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7842: 5v TTL input PWM(Vinl <0.8V, Vinh>2.0V), ISOM7842

Part Number: ISO7842
Other Parts Discussed in Thread: ISO7242C, ISO6742-Q1, ISO7741-Q1

Tool/software:

Hi,

A my account is search for a P2P compatible device with NSi8242W-DSWR which supports TTL input signal. The input voltage threshold of ISO7842 is for CMOS, is different, is any new one recommended?

Vcc=5V;

Input PWM signal is 5V TTL;