This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOUSB111: Does ISOUSB111 comply with the explosion-proof standard: IEC60079-11:2023, Section 7.10.2?

Part Number: ISOUSB111


Tool/software:

Dear Specialists,

My customer is considering TUSB111 for explosion proof equipment and has a question.

I would be grateful if you could advise.

--- 

I have questions about ISOUSB111.

① Is this device a non-optical signal isolator?

② If the answer to ① is yes, please let me know if the differential leakage current transfer limit under the worst-case data rate is 50uA.

(Reference: Excerpt from explosion-proof standard: IEC60079-11:2023, Section 7.10.2

Non-optical signal isolators, and optical isolators with intentional power transfer, shall comply with a differential leakage current transfer limit of 50uA,
under the most onerous conditions of data rate for the application under consideration, obtained from the manufacturer of the signal isolator.

---

I appreciate your great help in advance.

Best regards,

Shinichi