This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOW1432: ISOW1432: Controller interface via UART

Part Number: ISOW1432

Tool/software:

Hi,

We are interfacing ISOW1432 RS485 transceiver with MCU through UART interface UART TX- to D and UART RX to R, Please confirm this will work.

Also do we need to use flow control for these transceivers at MCU UART side.also for full duplex and half duplex option we can use DEand RE#.

  • RS-485 transceivers are commonly used with UARTs.

    Do you want to use full duplex or half duplex? For half duplex, you need to control DE with a separate GPIO.

  • Hi Divya,

    Please find my inputs below:

    We are interfacing ISOW1432 RS485 transceiver with MCU through UART interface UART TX- to D and UART RX to R, Please confirm this will work.

    Yes, this can work with appropriate connection of DE and /RE.


    Also do we need to use flow control for these transceivers at MCU UART side

    ISOW1432 is a full duplex capable device. Hence Flow Control is not needed in full duplex mode.


    also for full duplex and half duplex option we can use DEand RE#.

    I did not get your question here. I'm assuming you're asking about DE and /RE connection in full duplex vs half duplex. If yes then please refer section 11.1 in datasheet for understanding DE and /RE dependency on full duplex and half duplex.

    Regards
    Varun