Part Number: ISO7721
Tool/software:
Dear Team.
I'm using ISO7721DR and MAX13488 for RS485 communication.
Attached is the circuit diagram.

I checked that it is working, but there's a strange thing. As far as I understand, ISO7721 insulates what comes in as input and sends it out as output.
Then, according to my circuit, the TX of the CPU comes out, passes through ISO7721, goes into D of MAX13488. and the RX of the CPU goes through ISO7721 into R, right?
But it's weird that UART's RX and TX communicate without intersecting.
Isn't there a separate function that intersects inside ISO7721?
Best Regard,
Hyerin