Other Parts Discussed in Thread: ISO1450
Tool/software:
I’m using the ISO1452DW in a new design and having a strange issue; perhaps you can help me troubleshoot it. First, the schematic:

You can see that the 1.8V supply is powering the “inside” of the transceiver, and I have a separate, isolated 5V supply powering the outside. (actually it's 4.96V but close enough.)
I’m testing the 1452 driver side right now, which means I have pin 5 pulled high to 1.8V via a 100k resistor, as you can see in the lower left of the schematic screenshot. I’m feeding a 1kHz, 1.8V pulse train to pin 6, the driver input, and I expect to see differential outputs on pins 11 and 12. However, instead of this, I see two outputs that match the input phase exactly; there seems to be no complimentary output. The voltages seem reasonable, but both output pins are both the same phase. See scope plot below:

Any ideas what’s happening here?
Thanks, and have a great weekend!
Geoff (DTS)
Seal Beach, Ca