Part Number: ISO1540
Other Parts Discussed in Thread: TCA9517A
Tool/software:
Hello Team,
We are using the isolator ISO1540DR in one of our applications.
The master for the I2C is MSP432E401YTPDTR and the slave is INA238AIDGST.
According to the datasheet of the ISO1540DR, 

Does this mean the Vol at side 1 will not got to 0V.
According to the datasheet of the slave, the maximum Vil is 0.4V only.
Will this create any logic comparability issues?.
Attached the schematic for the same.

Also, in our case, the VCC1 is +5V and VCC2 is +3.3V.
will this create any problem?.