Part Number: ISO3082
Other Parts Discussed in Thread: TIDA-00333, , ISO1412, SN6501, ISO1410
Tool/software:
Dear Experts,
We are currently in search of an RS-485 half-duplex isolated design with auto direction control. After some research, we found the following link to a TIDA-00333, which offers complete isolation with automatic direction control for the RS-485 repeater. We plan to adopt half of this design for our own system, but before proceeding, we would like to discuss it with experts to reach a final decision.
Our requirements are as follows:
- The input voltage (3.3V) needs to be isolated. We are looking for the best and most upgraded solution for this.
- Auto direction control using a Schmitt trigger, such as SN74LVC2G14DBV.
- An isolated RS-485 IC, such as ISO3082.
- Protection for the transmission lines to handle the maximum possible conditions.
We would appreciate your expert feedback to ensure we are heading in the right direction.
Thank you for your time and support.
Best regards
Surya