This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1042-Q1: CAN to CAN isolator

Part Number: ISO1042-Q1
Other Parts Discussed in Thread: TIDA-01487

Tool/software:

Hi,

We are designing a carrier board for automotive application. For that we are looking for a CAN to CAN isolator which is mainly to seperates the CAN bus signal of the Automotive and our system.This ISO1042-Q1 IC seems to be a CAN tracevier which provides isolation between the CAN controller (TX, RX) and the CAN device (CANL, CANH). But we are looking for a CAN(CANH, CANL) to CAN(CANH, CANL) isolator.
Could you please suggest any IC for our requirement.