Part Number: ISO1228
Tool/software:
Hello,
I am interested in operating the ISO1228 in source mode, but would like to consider the possibility of increasing the current.
I see that the device supports Type 1 for 2.5mA and 3.5mA, and Type 2 for only 2.5mA (3.5mA is stated in table 8.2 as "not supported").
Question 1:
It is clear to me that Rpar can be changed in order to set the current...
- So, what is the consequence of adjusting Rpar until the device sources 5mA or 10mA of current, for example?
- I'm assuming it no longer conforms to IEC 61131-2, but is it safe to operate the device with higher currents, set by Rpar?
- Is there a way to characterize the voltage thresholds and behavior if this is done?
Question 2:
I am anticipating that Type 2 operation is one possible solution, and that two channels need to be connected in parallel.
- Is this supported in source mode?
- If using the parallel interface output, do I read the status of just one of the two OUTx lines, or connect them together?
Thank you in advance for your help.