Part Number: ISO1228DFBEVM
Other Parts Discussed in Thread: ISO1228, ISO1228EVM
Tool/software:
Hi everyone:
For the ISO1228DFBEVM, on its data sheet on the Table 1-1. it considers 16K for the RPAR.
However, on the Table 8-1. of the ISO1228 data sheet and also on the Table 1-1. of the ISO228EVM in both cases a 13K is considered for RPAR, being in all the 3 cases the same selection for Sink Mode and IL = 2.5mA.
What would be the reason for the difference? At first I thought maybe it was related to the LED selection, but both evaluation modules use the same 150060VS75000 LEDs.