This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1640: Design review and low temperature connection issue

Guru 11300 points
Part Number: ISO1640
Other Parts Discussed in Thread: INA238, , INA226

Tool/software:

Hello,

My customer designed an isolated I2C interface circuit using ISO1640 to interface with INA238 as shown below.

Q1. Please review the above circuit design to see if there are any problems.

Q2. They have an issue where I2C communication works fine at room temperature during board testing, but does not work at low temperatures.

       Here is the measurement of the I2C connection between the INA238 and the ISO1640:

       1) Room temperature(normal)

            

         2) Low temperature(about -20 degrees)

            

            Please advise on what causes this issue and how to fix it.

Thank you.

JH