Tool/software:
i follow the indication to use Wurth transformer PN 750319693 to have 24VDC out put voltage (12V input voltage).
the problem is that I have 27VDC as output voltage.
I have not use LDO because my input voltage is 12V from stabilized power supply.
what's the possible solution to have 24VDC?
why in datasheet do you write 12V to 24V with Wurth transformer PN 750319693? is not true.
i hope you can help me