Part Number: ISOM8110
Other Parts Discussed in Thread: ISO1212, ISO1228
Tool/software:
Hi
Could you help suggest suitable products to replace the following, Thanks
ACPL-247-500E
ACPL-227-500E
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Gareth,
Thanks for reaching out. This part looks to be a multichannel optocoupler. ISOM8110 is a single channel opto-emulator that is functionally equivalent to the ACPL part.
If this is for a digital input application (24V inputs), then ISO1212 and ISO1228 would be a good multichannel solution that we can provide.
What is the application that the ACPL part is used in?