Part Number: ISO1042
Tool/software:
Hi,
ISO1042DWVR is a isolated CAN transceiver.
In my particular application,
Vcc1 is constantly powered on and is connected to MCU (CAN tx-rx side)
To avoid any damage/malfunction to the devices on the live CAN-bus, Vcc2 (CAN H-L side) supply is being controlled by MCU and will only turn on when the device is properly docked in place and ready to communicate.
This case is not mentioned in datasheet. Not sure if powering on only Vcc1 will cause any damage to the IC or not. Please advice