Part Number: ISOW7742-Q1
Tool/software:
Hi,
I'm working on integrating the ISOW7742-Q1 into a design and would like to have the ability to change the output voltage of the isolated power converter from 3V3 to 5V or vice versa at runtime. What is the behavior of the IC when VSEL is changed during operation? My through process was to use one of the forward channels to control VSEL pin while the converter is running to get the desired output voltage. Will the change in voltage, especially going from 5V to 3V3 damage the isolator?
Thanks!