Part Number: ISO1640
Other Parts Discussed in Thread: TCA9517
Tool/software:
Hi everyone,
I'm working with an MCU(3.3V) as an I2C mater, and I need to isolate a segment of the bus to interact with:
1. one sensor(powered at 1.8V) for I2C signals
The background of the circuit design is like this, the sensor is undergoing EMS/EMC test, I need to read the data through I2C communication to monitor if the sensor is working properly.
so I need an isolation to isolate the RF interference.
now the problem is that the ISO1640 can't support the logic level of 1.8V; do you guys have any good ideas?
Thank you in advance for your help.