Part Number: ISO7740
Other Parts Discussed in Thread: ISO7240M
Tool/software:
Hi,
The datasheet specifies 100 Mbps as the maximum data rate. However, on page 7 it mentions the following "100 Mbps is the maximum specified data rate, although higher data rates are possible.". Do we know which data rates values it can still achieve and respective compromise on the parameters (propagation delay, skew, others...)? Is there additional documentation that complements this statement? There are other topics related to data rate, but not exactly regarding this question. When possible, I will test it, but would be good to know if there is information that I could already have as reference. Thanks in advance!
Best regards,
Luciano.