Part Number: SN6505A
Other Parts Discussed in Thread: SN6501,
Tool/software:
I need an isolated ±5V from 5V input with only few milliamperes of output current. I came across SN6501 and SN6505 and possible solutions seem:
1. SN6505A + Würth 750315240 which has 80% efficiency at 25mA, but there is no information for lower current.
2. SN6501 + Würth 750313638 has efficiency of 0-40% below 10mA.
It seems, SN6505 is designed for higher current. But can I expect similar efficiency also for the first option? Since we already use SN6505A in other products, I would prefer to use it if the performance is similar.
Does TI prefer one over the other, or is there any better solution you recommend with increasing the BOM?
Thanks!