Part Number: SN6507-Q1
Tool/software:
Hello team,
I have bulk capacitor at output and limitting the current using discrete circuit.
Input voltage is around 6V.
1. During normal operation input current is less than 0.5A but during the charging of capacitor it would be around 0.7A for 0.6s. Is it ok for this time?
2. Let's say current limit is set to 1.3A and if the current is around 0.7A for long time also will it work without any problem? (because power is less as input voltage is less)
Thank you,