This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1640: Power On Sequence

Part Number: ISO1640


Tool/software:

Hi,

Is there a power supply sequence for VCC1 and VCC2?
Based on the specifications in the data sheet, I don't think there are any restrictions on the power-on sequence.
However, I wanted to ask just to be sure because there is the following sentence:

D/S P34
"A strongly driven input signal can weakly power the floating VCC via an internal protection diode and cause undetermined output."

Best regards,
Hiroshi

  • Hi Hiroshi,

    Thanks for reaching out.

    Yes, you are right, there is no power sequence requirement for ISO1640.


    "A strongly driven input signal can weakly power the floating VCC via an internal protection diode and cause undetermined output."

    This Particular Sentence in datasheet explains about how there can be an undetermined state on Output channels in case of powered down state of VCCO.

    Regards
    Varun