This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1500: How can I use this device for an inline RS-485 isolation buffer

Part Number: ISO1500

Tool/software:

e2e, 

I'm working on a in line RS-485 isolator project with the below requirements:

Inputs:

  • V+ 24Vdc/4A – (Class 2 power supply)
    • GND
  • RS485 – A
  • RS485 – B

 

Outputs (isolated):

  • V+ 18 Vdc/250mA – (24 Vdc/250mA would be better)
    • GND
  • RS485 – A
  • RS485 – B

 

I was looking into the ISO1500 as a recommendation for this as the ISOW14xx devices wouldn’t have enough output power for this application. Is the ISO1500 what you would recommend for this?

 

Please let me know if you have any questions or need any more information.

Adam