Tool/software:
Similar to others I have ISOW1432 correctly wired, DE is low, EN is high, mode pin floating for 3.3V output. Isolated output measures 3.3V
There is no external connection, just 120R termination.
It draws 220mA from the 5V supply when idle and the thermal camera shows a hot spot near pins 11 and 12 that is at 55 degC which is more than 30 deg above ambient.
This seems wrong to me but I have spent a lot of time looking for errors in the layout and disconnecting the outputs.