Other Parts Discussed in Thread: UCC28740, UCC28910, PMP, UCC25230, UCC28C45, UCC28C43
Tool/software:
Hi TI Community,
I'm working on a project that requires a flyback converter with the following specifications, and I would appreciate any guidance or recommendations on TI parts, transformer design, and overall architecture.
-
Input Voltage: 10V to 30V DC
-
Outputs:
-
12V @ 2A
-
5V @ 4A
-
3.3V @ 2A
-
-
Topology: Isolated Flyback
-
Flyback Controller IC: I'm looking at parts like UCC28740, UCC28910, or any other TI-recommended controller for this power level and voltage range.
Questions:
-
Which TI controller IC would you recommend for this multi-output isolated flyback design (with wide Vin)?
-
Are there any reference designs or PMP examples close to these specs?
-
Should I regulate the 5V or 3.3V rail for best overall accuracy?
-
Is there a recommended method to post-regulate the 3.3V/5V outputs if I regulate only one rail directly?
Thanks in advance,
Shashank Reddy
Hardware Design Engineer