Part Number: ISO1228
Tool/software:
Hi all,
My customer are testing a prototype using ISO1228. It is used for both Sink and Source.
To save space, they do not use LEDs. All LED pins (LED1~8) are NC.
They can use them without any problem, but this causes a fault to be output.
1) Is it possible to use LED pins with NC (Non connected)?
2) I would like to send a circuit diagram. Could you tell me the person in charge?
Best Regards,
Ryusuke