Other Parts Discussed in Thread: ISO1042
Tool/software:
Hi everyone,
I am using ISO1042Q in few of the boards in my CAN architecture that contains 9 nodes (architecture will share you if required ). I getting BUS OFF the movement I send data from advantech board and no issues while receiving the data. However there is no issues if I remove Power board and battery node from CAN Bus.
The following nodes are battery ground:
1. Battery - unknown CAN transciever
2. Power board
3. Two motor controllers - unknown CAN transciever
Remaining are isolated grounds with ISO1042Q1 transciever
Note: Bus off because of TX errors going 252 . I have not connected all CAN grounds and only used CANH and L lines.
Please suggest correct method to debug this issue
Thanks in advance