This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1050: Isolation forum

Part Number: ISO1050


Tool/software:

ISO1050のパターンに関してCANの部分を等長配線にて設計中ですが

線長の許容値をご教示お願い致します。

例としてパターン配線長CAN_H 10mm,CAN_L 12mmだと2mmの差がでるがこれは問題ないのでしょうか?