Part Number: ISOW7742
Tool/software:
What is the minimum data rate for this component? Can it be used for static signals either high or low for long periods of time?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISOW7742
Tool/software:
What is the minimum data rate for this component? Can it be used for static signals either high or low for long periods of time?
Hi Brian,
Thanks for reaching out. Please find my inputs below:
Can it be used for static signals either high or low for long periods of time?
Yes, the ISOW7742 can support data rate as minimum as static high or low - for as long the application needs it to be across all voltage and temperature conditions
Also, the maximum supported speed is 100Mbps.
Regards
Varun