Part Number: ISO1042
Other Parts Discussed in Thread: SN74LVC2G17
Tool/software:

To save the power, we are thinking to shutdown supply to ISO1042 during sleep mode of uC.
There are 2 scenarios which can be implemented to save power.
1. Microcontroller (3V3_uC) in sleep mode, Vcc1(3V3) ON, Vcc2(5V_ISO) OFF
2. Microcontroller (3V3_uC) in sleep mode, Vcc1(3V3) OFF, Vcc2(5V_ISO) OFF
Do you think it can have impact on the IC in any of the above 2 scenarios, i mainly looked on the below table

Here when Vcc1 is 0V during off state, the limit is just 0+0.5V..i.e 0.5V??
Can i implement the above 2 scenarios without any issues?