How can pin A and pin B be protected so that the safety limitg values are complied with?
Inserting series resistors in the bus lines to protect the insulation barrier does not seem like a good idea to me.
Is there an internal protection to also protect pin A and pin B against over current / overload?
datasheet of ISO14xx (SLLSF22H – APRIL 2018 – REVISED JUNE 2024): "(2) ISO14xx is suitable for safe electrical insulation and ISO14xxB is suitable for basic electrical insulation only within the safety ratings. Compliance with the safety ratings shall be ensured by means of suitable protective circuits."