Other Parts Discussed in Thread: LM25037,
Tool/software:
Hi,
I’m designing a push-pull converter using the LM25037, and I would like to implement the isolation with an opto-emulator.
I read in the ISOM8110 datasheet that the minimum forward current is 0.5 mA.
The COMP pin of the LM25037 has an internal 5 kΩ pull-up resistor.
In steady-state, the voltage at the COMP pin is around 1.2 V, which means that approximately 760 µA flows through the ISOM8110’s output transistor.
Assuming a current transfer ratio (CTR) of 180%, the LED current would be around 422 µA — which is below the minimum 0.5 mA specified.
Is it possible to use the ISOM8110 with the LM25037?
Could I perhaps add a pull-up resistor to the COMP pin to increase the current through the transistor?