This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61047: Inductor and Input capacitor

Part Number: TLV61047

Tool/software:

Hi All,

I have a question about the TLV61047.

(1)When I performed the calculations according to 8.2.1.2.2 Inductor Selection, the inductor was 120uH.
VIN=12,VOUT=17V,IOUT=30mA
However, it states that the recommended capacitor is 4.7uH or 10uH.
Is it better to install 120uH as calculated, or 10uH?

(2)I also have a question about the input and output capacitors.
There is a formula for the output capacitor, but not for the input capacitor.
Is there a formula for the input capacitor? Or should I use the same formula as the output capacitor?


Best Regards,
Ishiwata