Tool/software:
Assuming a 5V supply that collapses rapidly when input power is removed, the device may be enabled or disabled.
When enabled, there will be energy stored in the transformer primary inductance as the 5V power rail source
drops to zero. How is this residual energy in the transformer handled by the device, as it could potentially result
in a large overvoltage on the 5V rail and subsequent ringing? Are clamp diodes needed between D1/D2 pins and
5V to prevent this?