Other Parts Discussed in Thread: ISO6721
Tool/software:
HI Team,
I have an application using ISO6721 as isolated UART, the OUTB is connect to an UART slave's RX pin. And when VCC= 0V on both side of the ISO6721, my device RX pin are internally pull up to 5V through a 230Kohm internal resistor. And I found that the RX pin is draining about 20+uA of the internal 5V. OUTB is about 1.1V. When I disconnect the OUTB from the device RX, the current is gone and OUTB return to 0V.
What's the state of the OUTB pin when no supply applied on the ISO6721, and why the OUTB is pulled up to 1.1V?
Thanks