Part Number: DCR010505
Tool/software:
I am using DCR010505U for isolated 5V output, for isolated transceivers.
There is a lot of ripple on all the digital output lines and 5_ISO line.
Below is the output from an optocoupler output.

This GND_ISO (connected to isolated ground of interfaces) is not connected to any other reference ground in the circuit and is left floating. If not connected, this noise is seen on 5V ISO line. If I connect this GND_ISO to Power ground or to the chassis, the ripples are no more seen. Shouldn't such isolated grounds be left floating?

I have a power ground (GND_P), isolated DC/DC converter that steps down this input to 5V (GND_D). After this I am using DCR module for Isolated power (GND_ISO) and it is picking up noise from ambient. This above snip is when I have just connected the DC jack of power supply to my device input, and the supply is not turned ON. Signal is from the output of an optocoupler When in application, this may get terminated at the other end depending on the application and end user. But for EMC tests and general testing of units, where should I connect this GND_ISO?