Other Parts Discussed in Thread: ISO7841, ISO6441, ISO6741,
Tool/software:
Is there a proven solution for using TI digital isolators to reliably operate across a 4-5kVDC continuous working voltage? The particular application is SPI.
The best parts that I found, like the ISO774x and ISO774xTA, have a VIOWM of 2121VDC. In this portion of the design, I believe we need only functional insulation, but with very good long term reliability. Based on the datasheet graph, the 1ppm TDDB for these parts at 4kVDC is on the order of a year.
An additional concern is power, both for the isolator(s), and the low power sensing circuit beyond it.
Thanks for any help you can provide.
Best regards!