Tool/software:
Hello team,
Can you support my customer's question as shown in below?
1. EN/FLT pin: Can this port use as EN or FLT? Cannot use as EN and FLT.
2. Is this 11.2 figure shows example use as FLT?
3. If they use as EN, they need to set extra GPIO from MCU side, is this correct?
4. Can they use as VDD=3.3V sharing with VIO?
5. I heard that the RS485 bus-side current exceeds 20mA. Is there any problem if an extra 20mA be inputed to the VISOIN?
6. If the EN/FLT port is not used as EN or FLT, what should the port handle?
Regards,
Youhei MIYAOKA