Tool/software:
We are using ISO3082 in our one application, we have not recevied any data and got fail RO pin in ISO3082 even we use SM712 diode for external protection purpose. Please help to get solution.
Regards
Dharmendra
Tool/software:
We are using ISO3082 in our one application, we have not recevied any data and got fail RO pin in ISO3082 even we use SM712 diode for external protection purpose. Please help to get solution.
Regards
Dharmendra
Hello Dharmendra,
Thank you for reaching out. I understand that the R pin of ISO3082 (the logic level receiver pin) may be failing in your application. Is this correct?
Best,
Andrew
Hi,
I understand that the R pin of ISO3082 (the logic level receiver pin) may be failing in your application. Is this correct?
- Yes.
Please describe how the failure is identified. Is the failure intermittent or persistent? Is the pin 'stuck' low?
- Card communication was fail after running of 1 month and i check in card RO pin high.
Please include a schematic capture of ISO3082 that shows how the diode is connected,
- where AVDD - 5V, VCC(485) - 5V
Please provide waveforms that show the inputs and outputs to the device. Include the D, R, A and B pins in the scope capture.
- waveform at pin A & B
- Waveform at R pin
...
Regards,
Dharmendra