Part Number: SN6501
Tool/software:
Hello TI,
I am having an issue with multiple SN6501 transformer drivers.
Below is a schematic,

The transformer driver is not switching D1 or D2.
I have connected a scope ground to 5V and CH1 to D1 and CH2 to D2. I am only seeing switching during power on and off.
I have replaced SN6501 three times all with the same result.
I have tried with the transformer (T201) and without the transformer each having the same result of only switching during power on and off.
I have tried different values of C201. (1uF, 10uF, and 0.1uF) No change.
Does any one have an idea as to why the SN6501 is not working?
Thanks,
Allan