Part Number: ISO6520
Tool/software:
Can these structures be relied upon to steer a small amount of continuous current, limited by a PW resistor (say 1mA to 5mA), should INx exceed Vccx+0.5?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO6520
Tool/software:
Can these structures be relied upon to steer a small amount of continuous current, limited by a PW resistor (say 1mA to 5mA), should INx exceed Vccx+0.5?

Hi Dan,
Thanks for reaching out.
The diodes you see in the above diagram are used for very short ESD transients. This means that these diodes protect the device from very short transients or overvoltage. The ESD voltage rating that the device supports is listed out in datasheet. Since the diode is not designed to be operated with a continuous current, it doesn't have a continuous current rating defined. If you have a continuous current present that will go into the input of the device, please keep external resistors to keep the current less than 1mA. This allows for the ESD diodes to not be as stressed.
This E2E provides a similar explanation:https://e2e.ti.com/support/isolation-group/isolation/f/isolation-forum/1001045/iso7742-q1-what-is-the-current-rating-of-esd-bypass-diode-at-input-pin/3698252?tisearch=e2e-sitesearch&keymatch=continuous%252525252525252520current#
Regards,
Aaditya V