This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOW1412: Half-duplex

Part Number: ISOW1412
Other Parts Discussed in Thread: ISO1412,

Tool/software:

Hi All,


A and Y are shorted, and B and Z are shorted to enable half-duplex communication.
I'm sometimes having trouble switching between transmit and receive in 485 communication.
When transmitting from ISO1412, set the DE and RE pins high.
When receiving, set the DE and RE pins low.
In this way, DE and RE are switched between transmit and receive.
Is there any need to consider the timing when switching?
For example, do I need to wait a few seconds after switching, etc.

Also, can you confirm that the following pin settings are correct?

EN/FLT=High
IN=GISOIN pull-down
OUT=Open
The MODE pin is set to open because VDD=VIO=3.3V.


Best Regards,
Ishiwata