Other Parts Discussed in Thread: TCAN3404
Tool/software:
We have a special application that link 3 MCU with CAN bus. 2 MCUs are on the same PCB( 2" by 2"), the other one is on a separate PCA only 3" away connected by a short cable. design requires low noise.
option 1, the transceiver use ISO1044.
Ground is shared. 5V DC is provided by a dedicated LDO( share same ground).
option 2,
use single 3.3V power transceiver, TCAN3404.
share ground, share 3.3V power by a dedicated LDO.
from the noise point of view. is it reasonable to assume the isolate chip will generate less noise to the system? I think the difference is ignorable because the ground are shared.
Best Regards,
David