Part Number: ISO6720
Tool/software:
Hi,
I have a fault feedback signal which works on pull-up mechanism in Inverter gate driver. Feedback voltage will be 5V during no-fault condition and will be 0V if fault occurs. I have to transfer this signal to microcontroller with Isolation. So can I use ISO6720 for isolation or can you provide any other feasible part. We need an isolation of 6kV.
Regards
ARCHIN N BABU