This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOUSB211: Power requirements

Part Number: ISOUSB211

We are using the ISOUSB211DPR in our design and are already providing 5V and 3.3V input supplies as per the typical application circuit. Could you please confirm if it is mandatory to provide an external 1.8V power supply, or if the device can operate normally without it in this configuration?