Part Number: ISO7810
Other Parts Discussed in Thread: ISOM8610
Hi Experts,
I need to have high speed I/O channels (min 1Mbps to max 10Mbps) that individually can be used as inputs or outputs. Each channel when used as output should source up to 300mA. Is there anything that can help me do this? Can any digital isolators work here? Any application notes for reference
Regards,
Marvin