Part Number: ISO7741-Q1
Other Parts Discussed in Thread: ISO7741, ISOUSB211, ISOUSB111
Hello together,
I want to use the ISO7741 for galvanic isolation of a SPI-Interface (and 2 other signals)
When input and output are not connected this works well for my transfer rate of 1MBaud.
But galvanic isolation also means that input and output may be directly connected.
For example input and output may be connected over 2 USB-Interfaces to the same PC for maintenance.
When I make bridge the input ans output part the communication over the ISO7741 stops and the power consumption rises.
My schematic is equal to the design in the datasheet.
So, did I make something wrong.
If the ISO7741 don't support this kind of connection, is there an alternative?
I only have the space for the SSOP case.
This is the reason why I can not use optocouplers.
Thanks for your answers !
Stefan Lauritzen