Part Number: ISO1042
Hi
Customer has a question: If VCC2 doesn't have an external power supply, can it be left unused?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
Yes, it can be. But I'm not sure what's the problem statement here.
But if VCC2 is not powered then there will be no CAN communication on Side2 of the isolator.
Regards
Varun
Hi Gareth,
VCC2 is the power source needed CAN Bus on ISO1042. If VCC2 is unpowered, CAN communication is not possible from the ISO1042.
Regards
Varun
Hi Varun
Another question regarding ISO1042: there are two packages, but in reality, not that many pins are needed. What are the advantages of choosing a 16-pin SOIC? Is there a difference between it and an 8-pin SOIC?
Thank you
Hello Gareth,
For these packages, there are no differences between electrical or isolation performance. 16-pin SOIC and 8-pin are both standard packages and 8-pin can be selected if you need the additional space in your design.
Best,
Andrew