This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN6507-Q1: Transformer selection

Part Number: SN6507-Q1
Other Parts Discussed in Thread: SN6507

Hello,

We are planing to use SN6507 with 750313638 to configure the below.

Input: 4.5 V to 6.5V

Output: 4.5V to 6.5V

Switching frequency: 400kHz

load current: 0.25A

Can we use above configuration, please let us know your comments.

image.png