This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6741-Q1: Enable from input side

Part Number: ISO6741-Q1
Other Parts Discussed in Thread: ISO6441

Hi team

Do we have digital isolator with Enable on the input side? this coudl help cusotmer save one buffer IC in their design,

 

Thanks

Scarlett

  • Hi Scarlett, 

    TI currently does not offer a digital isolator with input side enable pins. Our current isolators have the enable pin mainly on the output pins.

    Our suggestions for adapting this feature has been either using a buffer on the input side. Another option is to use our overvoltage tolerant inputs digital isolator, ISO6441, and turn off the input side power when no signal is needed. Even if the signal is present, the signal would not carry over to the output side when input power is off.

    Regards,
    Aaditya