Part Number: ISO6421
Hi TI Team,
I'm using ISO6421 in my isolated CAN application and utilizing its level shifting feature (3.3V to 5V translation).
Application Context:
I'll have two CAN-BUS variants:
- Isolated CAN (using ISO6421 with isolation)
- Non-isolated CAN (same PCB layout, different variant)
Question:
Can I use ISO6421 without its isolation function - purely as a level translator (3.3V to 5V) for the non-isolated variant?
This would allow us to use the same PCB design and component placement for both variants, only changing the population/configuration.
Is this a supported use case, or should I use a dedicated level translator for the non-isolated variant?
Regards